NOTICE: DDR Init Done NOTICE: BL2: v1.5(release):LSDK-20.12-dirty NOTICE: BL2: Built : 17:26:48, Dec 10 2021 NOTICE: BL31: v1.5(release):LSDK-20.12-dirty NOTICE: BL31: Built : 17:26:48, Dec 10 2021 NOTICE: Welcome to LS1012 BL31 Phase U-Boot 2020.04-dirty (Dec 10 2021 - 17:26:34 +0300) SoC: LS1012AE Rev2.0 (0x87040020) Clock Configuration: CPU0(A53):1000 MHz Bus: 250 MHz DDR: 1000 MT/s Reset Configuration Word (RCW): 00000000: 0800000a 00000000 00000000 00000000 00000010: 33050000 c000000c 40000000 00001800 00000020: 00800000 00000000 00000000 00014571 00000030: 00000000 18c2a120 00000096 00000000 DRAM: 958 MiB Using SERDES1 Protocol: 13061 (0x3305) MMC: FSL_SDHC: 0, FSL_SDHC: 1 Loading Environment from SPI Flash... SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB *** Warning - bad CRC, using default environment In: serial Out: serial Err: serial Model: LS1012A RDB Board Board: LS1012ARDB checkboard: Cannot find udev for a bus 0 Net: SF: Detected s25fs512s with page size 256 Bytes, erase size 256 KiB, total 64 MiB PFE class pe firmware for Linux PFE tmu pe firmware for Linux PFE class pe firmware for u-boot PFE tmu pe firmware for u-boot ls1012ardb_reset_phy: Cannot find udev for a bus 0 unsupported SerDes PRCTL= 13061 Could not get PHY for PFE_MDIO: addr 2 phy_connect failed unsupported SerDes PRCTL= 13061 Could not get PHY for PFE_MDIO: addr 1 phy_connect failed No ethernet found. Hit any key to stop autoboot: 0