U-Boot 2018.03 (Jan 04 2021 - 16:22:27 +0800) SoC: LS1043A Rev1.1 (0x87920111) Clock Configuration: CPU0(A53):1300 MHz CPU1(A53):1300 MHz CPU2(A53):1300 MHz CPU3(A53):1300 MHz Bus: 400 MHz DDR: 1300 MT/s FMAN: 500 MHz Reset Configuration Word (RCW): 00000000: 080d000d 0a000000 00000000 00000000 00000010: 24550002 80004002 40044000 c1002000 00000020: 00000000 00000000 00000000 00028800 00000030: 20044500 00001002 00000096 00000001 Model: LS1043A RDB Board Board: LS1043ARDB, boot from Invalid setting of SW4 CPLD: V0.0 PCBA: V0.0 SERDES Reference Clocks: SD1_CLK1 = 100.00MHZ, SD1_CLK2 = 100.00MHZ I2C: ready DRAM: Initialzing DDR using fixed setting Configuring DDR for 1300 MT/s data rate 1.9 GiB (DDR4, 32-bit, CL=11, ECC off) Using SERDES1 Protocol: 9301 (0x2455) PPA Firmware: Version LSDK-18.06 SEC Firmware: 'loadables' present in config loadables: 'trustedOS@1' ERROR: [0x0] TEE-CORE:tee_otp_get_hw_unique_key:195: H/W Unique key is not fetched from the platform. MMC: FSL_SDHC: 0 Loading Environment from SPI Flash... SF: Detected w25q128fw with page size 256 Bytes, erase size 4 KiB, total 16 MiB OK EEPROM: Read failed. In: serial Out: serial Err: serial #####scfg value is [1111] #####scfg value 2 is [0] SCSI: PCIe0: pcie@3400000 disabled PCIe1: pcie@3500000 Root Complex: no link PCIe2: pcie@3600000 Root Complex: no link Error: SCSI Controller(s) 1B4B:9170 not found Net: Invalid SerDes protocol 0x2455 for LS1043ARDB SF: Detected w25q128fw with page size 256 Bytes, erase size 4 KiB, total 16 MiB Fman1: Uploading microcode version 106.4.18 Could not get PHY for FSL_MDIO0: addr 0 Failed to connect FM1@DTSEC1 [PRIME], FM1@DTSEC2, FM1@DTSEC3, FM1@DTSEC4, FM1@DTSEC5, FM1@DTSEC6, FM1@DTSEC9 Hit any key to stop autoboot: 0 => mdio list FSL_MDIO0: 1 - AR8031/AR8033 <--> FM1@DTSEC3 2 - AR8031/AR8033 <--> FM1@DTSEC4 8 - Generic PHY <--> FM1@DTSEC1 9 - Generic PHY <--> FM1@DTSEC2 a - Generic PHY <--> FM1@DTSEC5 b - Generic PHY <--> FM1@DTSEC6 FM_TGEC_MDIO: =>