[ 210.023234] Unable to handle kernel execute from non-executable memory at virtual address ffffd791378bd948 [ 210.032900] Mem abort info: [ 210.035683] ESR = 0x000000008600000f [ 210.039422] EC = 0x21: IABT (current EL), IL = 32 bits [ 210.044724] SET = 0, FnV = 0 [ 210.047768] EA = 0, S1PTW = 0 [ 210.050899] FSC = 0x0f: level 3 permission fault [ 210.055680] swapper pgtable: 4k pages, 48-bit VAs, pgdp=00000000820b5000 [ 210.062371] [ffffd791378bd948] pgd=10000000fbdfe003, p4d=10000000fbdfe003, pud=10000000fbdfd003, pmd=10000000fbdf9003, pte=00780000828bdf03 [ 210.074890] Internal error: Oops: 000000008600000f [#1] PREEMPT SMP [ 210.081149] Modules linked in: crct10dif_ce fsl_qdma rtc_fsl_ftm_alarm [last unloaded: ip6_tables] [ 210.090111] CPU: 0 PID: 0 Comm: swapper/0 Tainted: G O 6.1.55+gd4bf94d51 #1 [ 210.098453] Hardware name: Aligera Mozart Board (DT) [ 210.103408] pstate: 400000c5 (nZcv daIF -PAN -UAO -TCO -DIT -SSBS BTYPE=--) [ 210.110362] pc : gic_data+0x0/0x648 [ 210.113851] lr : gic_data+0x0/0x648 [ 210.117332] sp : ffff800008003f90 [ 210.120637] x29: ffffd791378c7a80 x28: ffffd791378c7a80 x27: ffffd79136ec0070 [ 210.127768] x26: 0000000000000000 x25: 00000030e65c16f8 x24: 00000030e61fbe38 [ 210.134898] x23: ffffd791372889f8 x22: 000000000000000b x21: ffff222683029f80 [ 210.142029] x20: ffffd79136669400 x19: ffff222683020600 x18: 0000000000000000 [ 210.149159] x17: ffff4a95c431f000 x16: ffff800008000000 x15: 0000000000000000 [ 210.156289] x14: 000000000000003d x13: 00000000000000b1 x12: 0000000000000000 [ 210.163419] x11: 0000000000000000 x10: 0000000000000004 x9 : 0000000000000000 [ 210.170549] x8 : 00000030e62ae100 x7 : 7fffffffffffffff x6 : 00000001468b13da [ 210.177679] x5 : 00ffffffffffffff x4 : 0000000000cccccd x3 : 000019fd00067f40 [ 210.184809] x2 : 00000001468c27d8 x1 : ffffd791378c7a80 x0 : 0000000000000000 [ 210.191940] Call trace: [ 210.194378] gic_data+0x0/0x648 [ 210.197517] Code: 00000000 00000000 00000000 00000000 (08020000) [ 210.203602] ---[ end trace 0000000000000000 ]--- [ 210.208210] Kernel panic - not syncing: Oops: Fatal exception in interrupt [ 210.215074] SMP: stopping secondary CPUs [ 210.218991] Kernel Offset: 0x57912d080000 from 0xffff800008000000 [ 210.225074] PHYS_OFFSET: 0xffffddda00000000 [ 210.229246] CPU features: 0x00000,00900080,0000421b [ 210.234115] Memory Limit: none [ 210.237161] Rebooting in 5 seconds..