About sunye
About sunye
sunye
Contributor I
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
I used the chip TDA8034. Once i bought 6 chips, now there are 4 chips working well using the same board. The two left are not woking well. The appearance is that the level of OFFN signal is changed when the signal CMDVCC level is changed, at the same tim
on
NFC
.
06-08-2016
12:38 AM
Latest posts by sunye
Subject
Views
Posted
I used the chip TDA8034. Once i bought 6 chips, now there are 4 chips working well using the same board. The two left are not woking well. The appearance is that the level of OFFN signal is changed when the signal CMDVCC level is changed, at the same tim
NFC
641
06-08-2016
12:38 AM
View All
Community Statistics
Posts
1
Solutions
0
Kudos given
0
Kudos received
0
Member Since
06-08-2016
Contact Me
Online Status
Offline
Date Last Visited
08-29-2020
02:09 AM