All Activity

Vikrant A P
Greetings! I am using micro SD Card in my custom imx7d board in accordance with the reference of the imx7d Sabre board. The issue I am facing is I am getting the initial pulse of SD card detection on SD1_CLK pin, whereas our CD pin of SD card is tied to Ground. I am using uSDHC0 (default one/same as sabre) for the SD card. I also have checked the… (Show more)
in i.MX Processors
Peter Bain
Hi guys. I'm trying to implement a DSI to LVDS bridge for the iMX8QM. From searching here, the SN65DSI83 / 4 seem popular options on other iMX variants. From what I can see from the iMX8QM reference design documentation, the DSI outputs from the i.MX8QM are set by VDD_MIPI_DSI_DIG_1V8_3V3, so a minimum of 1V8. The SN65DSI83 has a max input voltage… (Show more)
in i.MX Processors
Social News
Eddie Vazquez
Hello community, I have several questions regarding capturing a single picture using CSI interface. I have set up parallel sensor and csi driver (mx6s_capture.c). Driver for camera was ported to use subdev and succesfully shows as subdev of csi.   When I try to use ./mx6s_v4l2_capture.out -d /dev/video0   It calls functions from sensor… (Show more)
in i.MX Processors
Matters Most
Terry Biberdorf
Click to view contentI just installed MCUXpresso V11.1 I created a new workspace and created a New Project based on the MK60DN512xxx10 controller.     I then select the MCUXpresso Config Tools>>Open Peripherals and I get the following error message:   It is clearly shown in the Project Explorer window that my project MCU chip is a MK60DN512xxx10   Why can't… (Show more)
Alice_Yang
The MCUXpresso Config Tools is installed without the data for MCUs and boards, and the data are download on demand via internet. So this article describes how to use MCUXpresso Config Tools with offline Computer.   There are two methods: - Copy and paste the data on computer; - Connect the internet when first using.   About the detail steps,…
in MCUXpresso Config Tools
Matters Most
Jose Alberto Reyes Morales
Click to view contentHi,   The FXAS2100x, is a small, low-power, yaw, pitch, and roll angular rate gyroscope with 16 bit ADC resolution. The full-scale range is adjustable from ±250°/s to ±2000°/s. It features both I2C and SPI interfaces.   Here is a Render of the FXAS2100x Breakout- Board downloaded from OSH Park:   Layout Design for this board:   In the…
in Sensors
Biyong Sun
This tool is also for emmc user partition mirror. Just give this tool the emmc files. The typical use case is for emmc mass production by emmc offline programming.   Ver 0.4.0 2/14/2017 Support Android 7 Nougat. AndroidSDCARDMirrorCreator_Version_0.4.0_02142017.tgz   Ver 0.3.2: 6/13/2016 Using static link simg2img…
in i.MX Processors
Matters Most
Mark Butcher
Click to view contentHi All   I am making my first attempt to use MCUXpresso to debug a target but presently is fails since it doesn't seems to load any code to the board and also doesn't seem to do behave normally when connected (I can't see what it does since it deletes the console window content) This is what i have done: 1. Tested an i.MX RT 1015 SDK reference… (Show more)
in MCUXpresso IDE
sarvani adabala
Hello, The below attachment is the code for UART with the input data as a character..But i need the input data to be a STRING...Can anyone please post the code for UART with input as a string using MK22D5.
in Kinetis Microcontrollers
Matters Most
Aviad Megira
Hey, I want to connect my circuit through "AD5933 Chip" to NFC by I2C connection, I looked at several products that have NFC technology, but I am not sure that those products are relevant to my project.   so I need to read the data from the I2C interface of AD5933: I thought maybe to use: but I am not sure this product can read values from… (Show more)
in NFC
peterurbanek
To do:   Implement a program that lets the 4 LEDs on the Tower toggle all together using the PIT Interrupt. For easy debugging, let the program run in the RAM.   * toggle period 0.5 s, * extract vector table and service routines in 'vector.c.   Hint: Use the 'arm_cm4.c and 'arm_cm4.h' from the freescale kinetis homepage, which include access…
in Kinetis Microcontrollers
Load more items