Skip navigation

News

Top & Trending
Rubens Junior
Dear,   I'm working on a project with the NXP i.MXRT1050 family MIMXRT1052DVL6B processor. For preliminary testing I'm using the MIMXRT1050-EVK development kit. For the initial tests we are using the SDX provided by NXP. The Kit has 3 types of flash memory (Hyperflash, QSPI and SD card), the default boot being done by Hyperflash, just as the
8

christopherjwhitting@gmail.com
I have recently bought the MIMXRT1010-EVK and have been playing around with it. I managed to get the SDK Samples loaded and debugger working. However, I now have the board in a state where it will no longer jump to the application; the program counter is stuck in the ROM boot loader section (e.g. 0x20b0cc). I have the Boot switches set to 10,
0
Top & Trending
Martin Dušek
Hi, I built release configuration of MKL25Z4 freedom_bootloader in NXP_Kinetis_Bootloader_2_0_0. The only change I did was modification of linker script:   MEMORY { m_interrupts (RX) : ORIGIN = 0x00000000, LENGTH = 0x00000100 m_bootloader_config (RX) : ORIGIN = 0x000003C0, LENGTH = 0x00000040 m_flash_config (RX) : ORIGIN =
4