Skip navigation

News

Top & Trending
Rakesh Patel
Hi,   As per below document, iMX8QXP: Use RPMSG to wake up M4 and A35    patch : L4.14.78_rpmsg_wakeup.patch is for only L4.14.78.   Is there any patch for L4.14.15 as I see there are many changes in rpmsg kernel changes and it looks like not easy to port L4.14.78 patch to L4.1.15?  
5

Zhang Kisen
Hi,    I,m using the Model-Based Design Toolbox MPC57xx Series, I followed the quick start guide with the uart_hello_world_mpc574xP.mdl example. However, after I click the code generate and build model button in Simulink, and pressed the RESET button, it showed that "Loss communication with CCP MCU. Please cycle power and
2