SRK_REVOKE

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

SRK_REVOKE

1,610 Views
dheerajr
Contributor II

Hi, 

   I am using an imx6sx board and I am currently simulating the condition whereby one of the private keys is compromised. Therefore, I am trying to revoke the SRK that I am using to authenticate the kernel and the u-boot. I referred to imx6sx application processor reference manual (pg 2828) and I would like to clarify what bits i need to set to revoke my first SRK out of the 4 SRKs that I generated (fuse prog 5 7 [? value to be set to reg]). 

Regards, 

Dheeraj

Labels (1)
0 Kudos
3 Replies

1,331 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dheeraj

for revocation usage one can check AN4581 Secure Boot on i.MX50,

i.MX53, and i.MX6 Series using HABv4 

https://www.nxp.com/docs/en/application-note/AN4581.pdf 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,331 Views
dheerajr
Contributor II

Hi Igor, 

   Thank you, I have managed to revoke SRK0 and my boot process is unsuccessful. However, I changed my csf file but I am still unable to secure boot using other 3 remaining keys. Below is my CSF file. May I know what exactly is going wrong?

CSF File

[Header]

Version = 4.0

Hash Algorithm = sha256

Engine Configuration = 0

Certificate Format = X509

Signature Format = CMS

Engine = ANY

[Install SRK]

File = "../../crts/SRK_1_2_3_4_table.bin"

Source index = 0

[Install CSFK]

File = "../../crts/CSF2_1_sha256_2048_65537_v3_usr_crt.pem"

[Authenticate CSF]

#Left blank because by doing so configuration is set to default

[Unlock]

Engine=CAAM

Features=RNG

[Unlock]

Engine = OCOTP

Features = SRK Revoke

[Install Key]

#authenticates and installs a public key for use in Authenticate Data command

Verification index = 0

Target index = 2

File = "../../crts/IMG2_1_sha256_2048_65537_v3_usr_crt.pem"

# Sign padded u-boot starting at the IVT through to the end with  

# length = 0x2F000 (padded u-boot length) - 0x400 (IVT offset) = 0x2EC00

# This covers the essential parts: IVT, boot data and DCD.

# Blocks have the following definition:

# Image block start address on i.MX, Offset from start of image file,

# Length of block in bytes, image data file

[Authenticate Data]   

Verification index = 2

Blocks = 0x877ff400 0x00000000 0x0006fc00 "../../../u-boot-imx6-boundary-v2017.07/u-boot.imx"

Regards, 

Dheeraj 

0 Kudos

1,331 Views
igorpadykov
NXP Employee
NXP Employee

Hi Dheeraj

one can look at sect.5.5 SRK Revocation older revision of app note,

it gives more details.

Best regards
igor

0 Kudos