Flashing NAND using i.mx6ull over Serial UART

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Flashing NAND using i.mx6ull over Serial UART

821 Views
srishan
Contributor III

Dear I.MX Community,

In my custom design we dont have USB or SD card,  but I need to flash the images using UART to NAND flash, Atleast I want to falsh the U-boot to NAND flash and then later over the network and NFS and flash the other images like dtb, zimage and rootfs

Could you please share the NXP procedure over for flashing the U-boot to NAND flash using UART

Kindly do the needful as early as possible, as I am stuck with this from past many days

Many Thanks in advance

Eagerly awaiting for your replies

Labels (2)
0 Kudos
1 Reply

528 Views
CarlosCasillas
NXP Employee
NXP Employee

Hi,

You could take a look at the links below regarding complementary information about implementation of UART serial downloader for i.MX processors:

https://www.nxp.com/docs/en/application-note/AN3996.pdf

https://community.nxp.com/docs/DOC-1639

https://github.com/boundarydevices/imx_usb_loader


Hope this will be useful for you.
Best regards!
/Carlos

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos