Hello everyone
I did the wrong thing with the SDA interface, just used the JTAG on the FRDM board for the wrong target. Now it is necessary to program again. I suppose it is enough to use again the JTAG and reprogram the small processor. but it does not work. The files I find are .bin and I don t know how to use with the KDS. Is there a way to build the .elf from the source code?? Or a valid suggestion to repair everything..
Suggestion needed
Thank You everyone
Pietro
Good morning
Thank You for following..
I always fit with the JTAG, so it is not usual for me to use the SDA for debugging.
But once I did the wrong thing and now the SDA uP is deleted.
I am using the FRDM-K64.
The situation now is some examples need the SDA as a serial port... but I have no more.
In the users guide the files are used as .elf format. The files I find for reflashing the the SDA are .bin.
I suppose the .elf files should be available.. I see the source code of the SDA, so I wander if I should
load everything as a project in KDS and build the elf file as for debugging.
It seems to me not necessary, I expect it should be simpler
Thank You
Pietro
Hi Pietro,
You update reprogram the OpenSDA firmware refer to below link:
Have a great day,
TIC
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello ,
So do you want to use external debugger or the OpenSDA ?
And could you please take a video or take a screenshot about your steps and error ?
Which board ?
About debug board or flashing on KDS, you can have a look at
"KDS_Users_Guide" ->2.5 Debugging Projects
2.6 Flashing from file
BR
Alice