1366x768 HDMI resolution support

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

1366x768 HDMI resolution support

1,383 Views
harishkumarts
Contributor I

Hi,

we are trying to get HDMI display 1366x768 resolution for a HDMI panel which supports only that resolution

https://www.chalk-elec.com/?page_id=1280#!/15-6-HDMI-interface-LCD-with-capacitive-touchscreen/p/381... 

 

Below given link is tried but it dint help much

iMX6 HDMI output 1366x768 resolution

Please help us in getting 1366x768  resolution output from HDMI

BTW we are using imx6q processor and android 7.1.2 version

Labels (4)
0 Kudos
1 Reply

687 Views
igorpadykov
NXP Employee
NXP Employee

Hi Harish

HDMI settings on that link was used for another monitor, so

it is necessary to find panel timings in panel datasheet which you are using

and adjust video mode parameters with that specific timings.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos