flash write and read/

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

flash write and read/

578 Views
guochunhua
Contributor II

Dear sir/ms.

I have made a program in codewarrior 10.7,the cpu is mc56f84789. In PE, I have met two problems, they are follows.

1. I have added a flash module in my program,but I can not read or write the flash correctly, can you give me an example that how I read or write the flash? It is wonderful if you can give me a video.

2. I have added eFlexPWM module, there is a fault in my program when the PWM fault pin is high level. If there is a fault, sometimes enter the fault interrupt,sometimes does not enter the fault interrupt, how can I set the fault pin to enter the fault interrupt ? or which options can I set to enter the fault interrupt? can you give me an example? It is wonderful if you can give me a video.

Best regards.

chunhua guo

0 Kudos
1 Reply

369 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Chunhua,

This is a duplicate question of

https://community.nxp.com/thread/469202 

We have support engineer already contacted you via that link.

Please have a look, if that's not clear, please contact the support engineer with reply.

BR

Jennie Zhang

0 Kudos