OS: fsl-yocto-L4.9.11_1.0.0
Disro: wayland
Image: fsl-image-validation-qt5-imx
Soc: imx6q
When I run the qt example app "texture"(actually any gui program) from the ssh login, there will be an error: Failed to create display (No such file or directory).
I found that weston running on tty7, if I stop weston: systemctrl stop weston,
and then run the command: weston --tty=[1~7] &, the qt example works fine.
So how to configure the init weston run correctly?
weston.service:
[Unit]
Description=Weston Wayland Compositor (on tty7)
RequiresMountsFor=/run
Conflicts=getty@tty7.service plymouth-quit.service
After=systemd-user-sessions.service getty@tty7.service plymouth-quit-wait.service
[Service]
User=root
PermissionsStartOnly=true
# Log us in via PAM so we get our XDG & co. environment and
# are treated as logged in so we can use the tty:
PAMName=login
# Grab tty7
UtmpIdentifier=tty7
TTYPath=/dev/tty7
TTYReset=yes
TTYVHangup=yes
TTYVTDisallocate=yes
# stderr to journal so our logging doesn't get thrown into /dev/null
StandardOutput=tty
StandardInput=tty
StandardError=journal
EnvironmentFile=-/etc/default/weston
# Weston does not successfully change VT, nor does systemd place us on
# the VT it just activated for us. Switch manually:
ExecStartPre=/usr/bin/chvt 7
ExecStart=/usr/bin/weston-launch -- --log=/var/log/weston.log $OPTARGS
IgnoreSIGPIPE=no
[Install]
WantedBy=multi-user.target
one can refer to the document as below, tell you how to build and run the weston on the imx6, hope helpful for you