Hi Yuri,
Thank you for the help, specially with the Miro Samek tutorial, i was able
to fix the problem but now i have a new question, didnt post it in the
thread because i assume this is something basic.
So far i've been using the u-boot to create the image.imx and the DD
command to load it to the SD card:
kernel.img : gcc.ld $(OBJS)
$(LD) $(OBJS) -T gcc.ld -o kernel.elf $(LDFLAGS)
$(OBJDUMP) -D kernel.elf > kernel.asm
$(MKIMAGE) -n imximage.cfg -T imximage -e 0x17800000 -d kernel.img
kernel.imx
But using this new project with a more complete linker and startup code
when using those methods the image doesn't run.
So i wanted to ask how can a load the image on the board without the u-boot.
i manage to create the .axf file (the format i found in the arm's examples)
and i wanted to ask how can i program the SD using this image.
I use this command to create the file and i made the debug using the DS5
and it works fine.
$(LD) $(OBJS) -T gcc.ld -o kernel.axf $(LDFLAGS)
By the Way i'm using linux.
Kind Regards,
Ailton Lopes
2017-09-25 10:12 GMT+01:00 Yuri <admin@community.nxp.com>:
NXP Community
<https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: SGI not working i.MX6QSD
reply from Yuri Muhin
<https://community.nxp.com/people/Yuri?et=watches.email.thread> in *i.MX
Community* - View the full discussion
<https://community.nxp.com/message/946229?commentID=946229&et=watches.email.thread#comment-946229>
Hello,
please look at the following https://community.nxp.com/docs/DOC-334664
Have a great day,
Yuri
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------