Question, video overlay, i.MX6Q-SDB

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question, video overlay, i.MX6Q-SDB

699 Views
SLICE
Contributor IV

Dear team,

My customer is trying to display with overlay, but it does not go as expected.

The customer is using i.MX6Q-SDB board, and they are using LinuxBSP(Yocto3.14.28).

They are using HDMI display port and decoded 1920x1080 video is flow out.

They want to overlay graphical data image which was drawn on fb1 to the HDMI output. When the resolution of fb1 is 1280x720, the overlaying goes as expected.

But when the resolution of fb1 was 1920x1080, then the overlaying did not work.

And the following warning messages were seen.

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_5 = 0x08000000

imx-ipuv3 2400000.ipu: IPU Warning - IPU_INT_STAT_10 = 0x00080000

BTW, fb0 has the same resolution(1920x1080) as fb1.

The information of fb0 is as below.

root@imx6qsabresd:/mnt/work# fbset -fb /dev/fb0 mode "1920x1080-60"

        # D: 148.500 MHz, H: 67.500 kHz, V: 60.000 Hz

        geometry 1920 1080 1920 3240 16

        timings 6734 148 88 36 4 44 5

        accel false

        rgba 5/11,6/5,5/0,0/0

endmode

 

Could you show me how to achieve that?

Labels (1)
0 Kudos
2 Replies

330 Views
joanxie
NXP TechSupport
NXP TechSupport

1) check if your hdmi can support 1080p or not

2)check if you set correct resolution in uboot

3) if you use fb0 for hdmi, does it work?

0 Kudos

330 Views
SLICE
Contributor IV

Hello joanxie

Thanks for your support.

My customer saw the following thread.

https://community.nxp.com/thread/429600

And they fixed this issue on their lab.

We can close this thread, thanks again.

Best Regards,

Miyamoto

0 Kudos