NAND two chips connection to i.MX53

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

NAND two chips connection to i.MX53

552 Views
ko-hey
Senior Contributor II

Hi all

 

Let me confirm about the connection of two NAND chips to i.MX53.

I understand that i.MX53 can connect four chips and want to connect two chips.

 

Are following connection correct ?

 

206267_206267.jpgimage003.jpg

 

Add info: I referred a following thread.

https://community.nxp.com/message/328462

 

 

Ko-hey

Labels (1)
0 Kudos
2 Replies

441 Views
igorpadykov
NXP Employee
NXP Employee

Hi Ko-hey

yes connections are correct and mentioned link provides correct info

from application team.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

441 Views
ko-hey
Senior Contributor II

Hi Igor

Thank you for quick reply.

Ko-hey

0 Kudos