Hi,
I use IMX6DL, Kernel3.14.52, Uboot2015.04. Now I'm porting one LCD which is LVDS port. Follow is its timing.
My device tree config is follow:
I also check waveform from scope , clock is 39.9MHz
The attach is my LVDS LCD display.
Anyone can help me solve this problem ?
Hi,
Thanks for your reply. I tested add <de-active> <pixelclk-active> <vsync-active > <hsync-active> and change diffrent value, but the result is same to previous test.
please also check similar issues on
LVDS output on Apalis i.MX6 (IXORA Board) - Toradex Community
Best regards
igor
Hi leavs
one can change fsl,data-width = <18>; and select appropriate kernel boot parameter
using Table 11. Common kernel boot parameters attached Release Notes,
try with nxp bsps described on
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi igorpadykov,
I had tested the data-width = <18>, but it didn't work. Do you have any other idea?