is it possible USB MSD in device mode in kl26z with 256KB of flash?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

is it possible USB MSD in device mode in kl26z with 256KB of flash?

356 Views
arthshah
Contributor II

hello kerryzhou

i have FRDM KL26Z board but i have replaced 128KB chip by 256KB of flash.

i have used USB MSD code from KL43Z and convert that code for my kl26z board now my program has no error but it stuck at some function,and program goes into default ISR.

usb_class_msc_init().

here i attached screenshot of my issue.usb_msd.png

0 Kudos
1 Reply

294 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi Arth Shah,

   After you modify the   FRDM KL26Z board with 256KB flash chip, please refer to the FRDM-KL46 USB MSD sdk code which can be downloaded from this link:

Welcome | MCUXpresso SDK Builder 

  The usb module in KL46 is the same as KL26.

  Please try it, if you still have problem about it, please kindly let me know!


Have a great day,
Kerry

 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos