Does Linux Kernel4.9.x and Android N7.1.2 support bt.1120 output?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does Linux Kernel4.9.x and Android N7.1.2 support bt.1120 output?

658 Views
takayuki_ishii
Contributor IV

Hello

A patch in the following, can support bt656 and bt1120 output Linux kernel 3.0.35 and Android JB4.2.

Patch to Support BT656 and BT1120 Output For i.MX6 BSP 

Does newer version of Linux 4.9.x and Android N7.1.2 BSP support bt656 and bt1120 output?

Or need to modify to do that?

It is described in the documents only bt656 and bt1120 input capture function.

Best regards,

Ishii.

Labels (4)
0 Kudos
2 Replies

413 Views
takayuki_ishii
Contributor IV

Hello

Victor

Thank you for your quick response.

I understand that are already supported.

Best regards,

Ishii.

0 Kudos

413 Views
b36401
NXP Employee
NXP Employee

The patch you noted is designed for old (3.0 and 3.1) kernels. In 4.9 one BT656 and BT1120 support should already be included.

Have a great day,
Victor

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos