IMX6q and Gstreamer : How to play smoothly a TS stream ?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6q and Gstreamer : How to play smoothly a TS stream ?

3,998 Views
fredericduchass
Contributor III

Hello,

I try using gstreamer on IMX6q (Yocto based OS) in order to play a TS stream. This stream is located on a closed network using UDP.

I use this pipeline:

gst-launch-1.0  udpsrc address=239.0.0.1 port=1234 buffer-size=20000000 ! tsdemux name=d program-number=257 ! multiqueue name=q use-buffering=1 d. ! q.  q. ! queue ! decodebin ! queue ! imxg2dvideosink q. ! queue ! decodebin ! queue ! audioconvert ! volume volume=10 ! alsasink

The program number 257 is H264 1080i @ 30fps video with ac-3 audio.

The problem is that using this pipeline, i get freeze sometimes and i get message from imxg2dvideosink about dropping frame because too late.

Have you got an idea about how i can improve my pipeline ?

(I try to delete all the queues but it's bader than before)

BR

Fred

Labels (4)
0 Kudos
13 Replies

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frederic

one can try with nxp gstreamer plugins using sect.7.3.13 RTP/UDP MPEGTS streaming

attached Linux Guide. Other documents can be obtained from linux documentation:

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS 

As imxg2dvideosink is part of gstreamer-imx plugins, it is supported by community and

issue may be posted on meta-fsl-arm mailing list, so that someone familiar with it could try to assist you.
https://lists.yoctoproject.org/listinfo/meta-freescale

Difference between community gstreamer-imx plugins and nxp gstreamer plugins described on

trac.gateworks.com/wiki/Yocto/gstreamer

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

2,606 Views
fredericduchass
Contributor III

root@apalis-imx6:/home# gst-launch-1.0 udpsrc do-timestamp=false uri=udp://239.0.0.1:1234 caps="video/mpegts" ! aiurdemux streaming_latency=400 name=d ! queue ! decodebin ! queue ! imxg2dvideosink
Setting pipeline to PAUSED ...
Pipeline is live and does not need PREROLL ...

====== AIUR: 4.0.9 build on Oct 11 2017 10:52:36. ======
Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.47 build on Feb 3 2016 05:52:16
file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1
Setting pipeline to PLAYING ...
New clock: GstSystemClock
Mpeg2CreateParser:parser created successfully
------------------------
Track 00 [video_0] Enabled
Duration: 0:00:00.000000000
Language: und
Mime:
video/x-h264, parsed=(boolean)true, alignment=(string)au, stream-format=(string)byte-stream, width=(int)176, height=(int)144, framerate=(fraction)30/1
------------------------
------------------------
Track 01 [audio_0] Enabled
Duration: 0:00:00.000000000
Language: fre
Mime:
audio/eac3, channels=(int)2, rate=(int)44100, bitrate=(int)0
------------------------
------------------------
Track 02 [audio_1] Enabled
Duration: 0:00:00.000000000
Language: qad
Mime:
audio/eac3, channels=(int)2, rate=(int)44100, bitrate=(int)0
------------------------
------------------------
Track 03 [audio_2] Enabled
Duration: 0:00:00.000000000
Language: qaa
Mime:
audio/eac3, channels=(int)2, rate=(int)44100, bitrate=(int)0
------------------------
[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0
[INFO] bitstreamMode 1, chromaInterleave 0, mapType 0, tiled2LinearEnable 0

In Fact, my video stream is 1920x1080i@25fps H264.

0 Kudos

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frederic

 

what bsp used in the case, one can try with nxp releases described in i.MX_Yocto_Project_User's_Guide.pdf

Table 1. Freescale Yocto project images included in doc package

https://www.nxp.com/webapp/Download?colCode=L4.1.15_2.1.0_LINUX_DOCS 

Best regards
igor

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

I don't really know if it's a clue  but i try to read buffer level when I see problems on the screen :

bufferdecodebinvideo level : 1995915
buffervideo level : 7311362
bufferdecodebinaudio level : 0
bufferaudio level : 540672
bufferdecodebinvideo level : 1792253
buffervideo level : 7311362
bufferdecodebinaudio level : 0
bufferaudio level : 602112
bufferdecodebinvideo level : 2160186
buffervideo level : 3655681
bufferdecodebinaudio level : 0
bufferaudio level : 577536
bufferdecodebinvideo level : 2151265
buffervideo level : 0
bufferdecodebinaudio level : 0
bufferaudio level : 565248
bufferdecodebinvideo level : 2033225
buffervideo level : 3655681
bufferdecodebinaudio level : 0
bufferaudio level : 552960
bufferdecodebinvideo level : 2153602
buffervideo level : 0
bufferdecodebinaudio level : 0
bufferaudio level : 540672
bufferdecodebinvideo level : 2028605
buffervideo level : 3655681
bufferdecodebinaudio level : 0
bufferaudio level : 589824

SO I can conclude that the buffer after video decoding can be empty sometimes. 

So the problem come from video decoder ? 

Have you got an idea ?

BR

Frederic

0 Kudos

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frederic

if you are using bsp from toradex, this may be posted on toradex support,

as it uses community gstreamer-imx plugins which are different from nxp gstreamer plugins

Toradex - Customer Support 

more about differencies in trac.gateworks.com/wiki/Yocto/gstreamer

Best regards
igor

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

I've asked to Toradex to look at this post. I  hope we will find a solution 

:-((((((((

Setting debug level of IMX, i can get these messages :

0:02:44.228679353 369 0x9472f0 DEBUG imxvpuapi imxvpuapi_vpulib.c:2171:imx_vpu_dec_decode: not enough input data was available
0:02:44.228850353 369 0x9472f0 DEBUG imxvpudecoder decoder.c:581:gst_imx_vpu_decoder_handle_frame:<imxvpudecoder0> input gstframe is incomplete; discarding this gstframe
0:02:44.281267019 369 0x9472f0 DEBUG imxvpuapi imxvpuapi_vpulib.c:2171:imx_vpu_dec_decode: not enough input data was available
0:02:44.281410353 369 0x9472f0 DEBUG imxvpudecoder decoder.c:581:gst_imx_vpu_decoder_handle_frame:<imxvpudecoder0> input gstframe is incomplete; discarding this gstframe

Can you explain me what it means ?

BR

Frederic

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

Can you help me to debug my problem please ?

I send the question to Toradex but i get no news...

Now i get this message debugging imxvpudec : 

0:00:43.572198005  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpudecoder decoder.c:581:gst_imx_vpu_decoder_handle_frame:<imxvpudecoder0> [00m input gstframe is incomplete; discarding this gstframe
0:00:43.608671672  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpuapi imxvpuapi_vpulib.c:2171:imx_vpu_dec_decode: [00m not enough input data was available
0:00:43.608792339  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpudecoder decoder.c:581:gst_imx_vpu_decoder_handle_frame:<imxvpudecoder0> [00m input gstframe is incomplete; discarding this gstframe
0:00:43.648815672  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpuapi imxvpuapi_vpulib.c:2171:imx_vpu_dec_decode: [00m not enough input data was available
0:00:43.648937339  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpudecoder decoder.c:581:gst_imx_vpu_decoder_handle_frame:<imxvpudecoder0> [00m input gstframe is incomplete; discarding this gstframe
0:00:43.688845005  [332m 1357 [00m 0xcb8690  [37mDEBUG  [00m  [00m imxvpuapi imxvpuapi_vpulib.c:2171:imx_vpu_dec_decode: [00m not enough input data was available

Do you know the meaning ?

Thanks in advance

Frederic

0 Kudos

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frederic

one can try with nxp plugins, check

How to install the fsl codec on linux? 

Best regards
igor

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

OK I'll try with nxp plugin (toradex image < 2.5) and I'll keep you updated.

Best regards

Frederic

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

Using gstreamer0.1 I find other problems  : aiurdemux can work with some TS but it doesn't work with others !

I use this pipeline to check :

gst-launch-0.10 udpsrc filesrc location=/home/TNT_M6.ts ! "video/mpegts" ! queue ! aiurdemux streaming_latency=400 name=d d. ! queue max-size-time=0 ! vpudec ! imxv4l2sink

this is the log :

root@apalis-imx6:/home# gst-launch-0.10 udpsrc filesrc location=/home/TNT_M6.ts ! "video/mpegts" ! queue ! aiurdemux streaming_latency=400 name=d d. ! queue max-size-time=0 ! vpudec ! imxv4l2sink
[ 1420.389823] ERROR: v4l2 capture: slave not found! V4L2_CID_HUE
[ 1420.395747] ERROR: v4l2 capture: slave not found! V4L2_CID_HUE
[ 1420.401603] ERROR: v4l2 capture: slave not found! V4L2_CID_HUE
MFW_GST_V4LSINK_PLUGIN 4.0.3 build on Oct 25 2017 12:12:13.
Setting pipeline to PAUSED ...
[INFO] Product Info: i.MX6Q/D/S
vpudec versions :)
plugin: 4.0.3
wrapper: 1.0.58(VPUWRAPPER_ARM_LINUX Build on Oct 25 2017 12:03:31)
vpulib: 5.4.28
firmware: 3.1.1.46063
0:00:00.115699333 788 0xb82cc0 DEBUG aiurdemux /media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c:1908:gst_aiurdemux_handle_sink_event:<d> Pushing newseg update 0, rate 1, applied rate 1, format 3, start 0:00:00.000000000, stop 0:00:00.024107616
Pipeline is live and does not need PREROLL ...
Aiur: 4.0.3
Core: BLN_MAD-MMLAYER_MPG2PARSER_04.04.26 build on Jan 20 2015 01:05:12
mime: video/mpeg, mpegversion=(int)[1,2]; video/mpegts, systemstream=true; video/x-cdxa
file: /usr/lib/imx-mm/parser/lib_mpg2_parser_arm11_elinux.so.3.1
Content Info:
URI:
file:///home/TNT_M6.ts
Idx File:
/home/root/.aiur/.home.TNT_M6.ts.aidx
Seekable : Yes
Size(byte): 24107616

Setting pipeline to PLAYING ...
New clock: GstSystemClock
0:00:00.121037333 788 0xb82cf0 WARN aiurdemux /media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c:2358:aiurdemux_loop_state_init: API[createParser2] failed, ret=-1
0:00:00.121144333 788 0xb82cf0 LOG aiurdemux /media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c:2359:aiurdemux_loop_state_init:<d> aiurdemux_loop_state_init create using createParser2 flag=4
0:00:00.121207000 788 0xb82cf0 LOG aiurdemux /media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c:4450:aiurdemux_push_task:<d> pausing task, reason error
0:00:00.121285666 788 0xb82cf0 WARN aiurdemux /media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c:4465:aiurdemux_push_task:<d> error: streaming stopped, reason error
ERROR: from element /GstPipeline:pipeline0/GstAiurDemux:d: GStreamer encountered a general stream error.
Additional debug info:
/media/sefram/7f7dd387-2c00-4810-babd-e0d994a86f25/oe-core/build/out-glibc/work/apalis_imx6-angstrom-linux-gnueabi/gst-fsl-plugin/4.0.3-r0/gst-fsl-plugins-4.0.3/src/parser/aiur/src/aiurdemux.c(4465): aiurdemux_push_task (): /GstPipeline:pipeline0/GstAiurDemux:d:
streaming stopped, reason error
Execution ended after 2428000 ns.
Setting pipeline to PAUSED ...
Setting pipeline to READY ...
Setting pipeline to NULL ...
Total rendered:0
Freeing pipeline ...
[--->FINALIZE v4l_sink
[--->FINALIZE aiurdemux
root@apalis-imx6:/home#

This is the link you can find my TS if you want to check:

https://drive.google.com/file/d/0B-hlgYw-WA9bb0VmMXJNc2lXa28/view?usp=sharing

BR

Frederic

0 Kudos

2,606 Views
igorpadykov
NXP Employee
NXP Employee

Hi Frederic

GStreamer 0.10 is not supported in latest bsps, please try with GStreamer 1.0

description in attached file.

Best regards
igor

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hello Igor,

I'm working on Toradex Apalis Imx6q module. So i use the BSP toradex. 

I also tried the Boot2Qt image for this module and same problem.

BTW : I don't really know if it's a good idea to use "aiurdemux". It seems to be depeciated because it has a lot of problems. But as i see in the documentation you gave me, the only big difference (compared with my pipeline) is the use of aiurdemux : 

$GSTL udpsrc do-timestamp=false uri=udp://10.192.241.255:10000 caps="video/mpegts"
! aiurdemux streaming_latency=400 name=d d. ! queue ! vpudec
! queue ! overlaysink sync=true d. ! queue ! beepdec ! pulsesink sync=true

Best regards

Frederic

0 Kudos

2,606 Views
fredericduchass
Contributor III

Hi Igor,

First thanks a lot for your answer.

Reading the specified chapter, i've seen that aiurdemux was not included in my Yocto image. So i've added the correct recipe to get aiurdemux.

Now i can use "aiurdemux" in my pipeline. But i always have a problem. At the output of aiurdemux, caps of the stream gives me a wrong size for width and height.and so, the decoding is bad....

Have you got an idea about why aiurdemux give me wrong width and height for my stream ???

Frederic

0 Kudos