I’m trying to use the ioctl call to an sdcard to search for a filename and then delete it. When the function call returns it has an illegal ram address in the structure. After digging for several days I have collected some information on the problem.
/* MFS part of the software */
MFS_SEARCH_DATA search_data;
MFS_SEARCH_PARAM search;
char filepath[46] = "";// used for the input filename wildcard
char filename_buffer[46]; // returned filename
search.ATTRIBUTE = MFS_SEARCH_LFN;
search.WILDCARD = filepath;
search.SEARCH_DATA_PTR = &search_data;
search.LFN_BUF = filename_buffer;
search.LFN_BUF_LEN = sizeof(filename_buffer);
search. SEARCH_DATA_PTR->ATTRIBUTE = MFS_SEARCH_LFN;
search.SEARCH_DATA_PTR->LFN_BUF = filename_buffer;
search.SEARCH_DATA_PTR->LFN_BUF_LEN = sizeof(filename_buffer);
// Check to see if this file exists. If so then delete it before creating a new one
sprintf(filepath, "snapshot%d_*.bin", file_index.intervention_snapshot_file); // wildcard filename
error_code = ioctl(a_fd, IO_IOCTL_FIND_FIRST_FILE, &search);
if(error_code == MFS_NO_ERROR)
{
sprintf(int_snapshot_file_name, "%s", search.SEARCH_DATA_PTR->LFN_BUF);
}
while(error_code == MFS_NO_ERROR)
{
error_code = ioctl(a_fd, IO_IOCTL_DELETE_FILE, int_snapshot_file_name);
error_code = ioctl(a_fd, IO_IOCTL_FIND_NEXT_FILE,search.SEARCH_DATA_PTR); // Check if there are more
if(error_code == MFS_NO_ERROR)
{
sprintf(int_snapshot_file_name, "%s", search.SEARCH_DATA_PTR->LFN_BUF);
}
}
A look at the addresses of the structure before and after the function call:
Just before the call to error_code = ioctl(a_fd, IO_IOCTL_FIND_FIRST_FILE, &search);
(Had to create variables to read addresses because the Expressions window was giving a different value than when I did a mouse over). These values are from MFS_SEARCH_PARAM.
a = (uint32_t)&search.SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.WILDCARD;
b = (uint32_t)&search.SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.ATTR_ONE_MASK;
c = (uint32_t)&search.SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.ATTR_ZERO_MASK;
d = (uint32_t)&search.SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.DIR_CHAIN_LOC;
e = (uint32_t)&search.SEARCH_DATA_PTR->LFN_BUF; = 0x20012fc6
After stepping into the file mfs_find.c and function _mfs_error MFS_find_init( MFS_DRIVE_STRUCT_PTR drive_ptr,
MFS_SEARCH_PARAM_PTR sp_ptr,
MFS_SEARCH_DATA_PTR sd_ptr):
The sp_ptr pointer is pointing to the same address as "search" from above.
a = (uint32_t)&sp_ptr->SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.WILDCARD;
b = (uint32_t)&sp_ptr->SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.ATTR_ONE_MASK;
c = (uint32_t)&sp_ptr->SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.ATTR_ZERO_MASK;
d = (uint32_t)&sp_ptr->SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.DIR_CHAIN_LOC;
e = (uint32_t)&sp_ptr->SEARCH_DATA_PTR->LFN_BUF;
In sp_ptr->SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.DIR_CHAIN_LOC you can see that address of this element of the structure MFS_SEARCH_PARAM is two bytes different than in search.SEARCH_DATA_PTR->INTERNAL_SEARCH_DATA.DIR_CHAIN_LOC (0x20012f9e vs 0x2001fa0)
When the line sd_ptr->LFN_BUF = sp_ptr->LFN_BUF; is reached (in MFS_find_init()) it copies the filename to 0x20012fa0 and when it returns to the calling function the variable “search” looks for the filename in 0x20012f9e resulting in a shift of the contents of LFN_BUF.
Any ideas why this is happening?
Solved! Go to Solution.
Solution: I recently split my .h files into prototype.h and struct.h because I was having problems with circular references. In my new struct.h file I added an #include for another .h file which contained a #pragma pack(1) directive. This would have been ok except there was not corresponding #pragma pack() to turn off the packing so my new .h file inherited the pack command and the MFS_SEARCH_PARAM search and MFS_SEARCH_DATA search_data were packed to a one byte alignment. Unfortunately the mfs.a library file had the default alignment, so this is what caused the alignment problem. I changed to using the #pragma pack(push, 1) coupled with a #pragma pack(pop). This cleared up the alignment problem.
Solution: I recently split my .h files into prototype.h and struct.h because I was having problems with circular references. In my new struct.h file I added an #include for another .h file which contained a #pragma pack(1) directive. This would have been ok except there was not corresponding #pragma pack() to turn off the packing so my new .h file inherited the pack command and the MFS_SEARCH_PARAM search and MFS_SEARCH_DATA search_data were packed to a one byte alignment. Unfortunately the mfs.a library file had the default alignment, so this is what caused the alignment problem. I changed to using the #pragma pack(push, 1) coupled with a #pragma pack(pop). This cleared up the alignment problem.
Thank you for your sharing.
Regards
Daniel