IMX6Dual: FROM SOC RESET TO START UBOOT,SPEND A LOT OF TIMES
Hi,ALL,
we use imx6dual auto meter project, we hope the meter startup very fast,but we encounter a problem,
that is from the imx6dual reset sigal to the start the uboot, spend more than 200 milliseconds test it by oscilloscope,we can not accept the result,and we do not think it make sense.
we hope NXP can support us, how long it takes(from soc reset to start uboot) gerenal?
And Is there a technical documentation?
Solved! Go to Solution.
Hi shalan
ROM uses the 32.768 kHz clock and 32.768 KHz crystal requires hundreds of ms
for start-up. As workaround one can try to boot from SPI-NOR initially ( it does not
require stable clock as suggested in ERR007926 description) then switch to other
boot device. Also may be useful to check
Linux Fast Boot on i.MX6Q Board: Building Steps
Boot an i.MX6 in 0.58 seconds - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hi ,igorpadykov,
thanks for you answer, you means ,if we boot from emmc , it must spend hundreds of ms to startup uboot.
Hi shalan
ROM uses the 32.768 kHz clock and 32.768 KHz crystal requires hundreds of ms
for start-up. As workaround one can try to boot from SPI-NOR initially ( it does not
require stable clock as suggested in ERR007926 description) then switch to other
boot device. Also may be useful to check
Linux Fast Boot on i.MX6Q Board: Building Steps
Boot an i.MX6 in 0.58 seconds - Boundary Devices
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------