KDS m_data segment overflow

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

KDS m_data segment overflow

1,821 Views
utsavikalpesh
Contributor V

Hello,

I am working with KDS with Towerkit TWR0K60D100M. I created my project in Processor expert mode.

By building my project using SysV format. I got like below,

section                          size                          addr

.interrupts                       1024                              0

.flash_config                      16                         1024

.text                           129716                         1040

.ARM                                 8                       130756

.init_array                           4                       130764

.fini_array                           4                       130768

.data                              904                   536806400

.m_interrupts_ram         1024                   536805376

.bss                           67300                   536807328

.heap                          53252                  536874628

.stack                            512                   536927880

.ARM.attributes                42                                 0

.debug_info               507910                                 0

.debug_abbrev            74434                                 0

.debug_loc                228149                                 0

.debug_aranges           12400                                 0

.debug_ranges             15624                                 0

.debug_macro            349650                                 0

.debug_line                339463                                 0

.debug_str               1972414                                 0

.comment                       112                                 0

.debug_frame              37204                                 0

.stab                              156                                 0

.stabstr                          387                                 0

Total                       3791709

 

What is this Total bytes? why it is too much large?? Beyond the range of RAM? 

When I print size unsing Berkley format , I got like this,

text                      data                   bss               dec                 hex          filename

0x1fecc           0x390         0x1dce8       253764         3df44     Test_Project.elf

bss + data =   0x1dce8 + 0x390  =  123000 bytes used.

Total RAM available is 128KB in module. 

When I manually calculate the ram like, structures used in my project, global variables and task stacks , Total RAM I calculate is only 37000 bytes.

Now when I declared, say array of 9000 bytes , I am getting error like, "m_data segment overflow by 986 bytes....."

why this is so?  

Tell me how can I find  Current Free RAM? In codewarrior I was using below functions, but I was unable to find this in KDS.  

_mqx_get_initialization() and ()_mem_get_free()

Regards

Utsavi Bharuchwala

0 Kudos
6 Replies

1,400 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Utsavi Bharuchwala,

1. "Total RAM available is 128KB in module. " 

While the SRAM is split into two equally-size logical arrays, SRAM_L and
SRAM_U, so on your chip each one is 64KB. Please check the default linker file "ProcessorExpert.ld",:

pastedImage_1.png

 the .data and .bss part all placed into m_data, not use m_data_20000000.

So "bss + data =   0x1dce8 + 0x390  =  123000 bytes used." 123000 > 64KB , overflow.

2. Please check the *.map file under your project->debug why the bss is so large.

About the bss in Eclipse please check this thread:

text, data and bss: Code and Data Size Explained | MCU on Eclipse 

3.In  your project, please don't use printf() print to console view, it adds greatly to

the code size of application and stack.

4.You can relocate the large data into the second RAM " m_data_20000000"

refer to : Relocating Code and Data Using the KDS GCC Linker File for Kinetis 

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,400 Views
utsavikalpesh
Contributor V

Hi Alice,

I have 

const int_16 Buffer[8000]; //changing approx 15 times per month

This buffer store in Flash as a RAM, but i want to know  limit of  Flash write  cycle? What is a life of flash memory?

Can I use Flash as RAM in this case?

Regards

Utsavi Bharuchwala

0 Kudos

1,400 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

 Hello Utsavi,

1. In your linker file , the two RAM part SRAM_L and SRAM_U have merged  to one m_data (RW) .

2.About the method of store huge arrays into flash memory, please also refer to this DOC:

Relocating Code and Data Using the KDS GCC Linker File for Kinetis 

3.About the Flash life cycle , please check on the Data Sheet of your chip:

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,400 Views
utsavikalpesh
Contributor V

Hello Yang,

Thanks for information.

In linker file, HEAP_SIZE = DEFINED(__heap_size__) ? __heap_size__ : 0xD000;
STACK_SIZE = DEFINED(__stack_size__) ? __stack_size__ : 0x0200;  What is that indicating??

When I tried to reduce heap size from 0XD000 to 0xC000 error of heap overflow error is solved....!! But my code is not running in this case what to do?

I am not using any malloc or calloc functions in my project, but I am assuming that the internal files may be using it. But my query here is why large size heap is defined? 

When I am declaring it as 0x0000, it is not giving me an error. Then what is the purpose of it?? 

Is it the right method to solve?? 

Regards

Utsavi Bharuchwala

0 Kudos

1,400 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hi Utsavi,

Maybe the  Heap is too big to other data overflow RAM, so when you reduce the Heap size there is no error .

BR

Alice

0 Kudos

1,400 Views
utsavikalpesh
Contributor V

Hi Yang ,

Thanks for reply. 

I can see that my bss start address is :  0x1fff07a0 and bss end address is : 0x200012e4  in .map file, so total bytes in bss is 68420.

And in between this bss range, variables are mapped.There is something like (*COMMON) segment which are also included in bss. what is that? 

One more thing there is no separate m_data_20000000 segment provided in my linker file. Segment in linker file is,

MEMORY {
m_interrupts (RX) :           ORIGIN = 0x00000000, LENGTH = 0x00000400
m_flash_config (RX) :       ORIGIN = 0x00000400, LENGTH = 0x00000010
m_interrupts_ram (RW) :  ORIGIN = 0x1FFF0000, LENGTH = 0x00000400
m_text (RX) :                    ORIGIN = 0x00000410, LENGTH = 0x0007FBF0
m_data (RW) :                  ORIGIN = 0x1FFF0400, LENGTH = 0x0001FC00  /*(130048 bytes)*/

How can I reduce bss size in KDS? How can I store huge arrays into flash memory if possible?

Regards

Utsavi Bharuchwala

0 Kudos