yocoto No command 'hob' found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocoto No command 'hob' found

1,980 Views
zhilinhuang
Contributor III

你好,我想运行hob :发现没有发现命令;

也是参考这样弄,是哪里出了问题吗,请求支持谢谢。

https://community.nxp.com/docs/DOC-102505 

imx6@ubuntu:fsl-release-bsp$ source setup-environment bld-fb/

Welcome to Freescale Community BSP

The Yocto Project has extensive documentation about OE including a
reference manual which can be found at:
http://yoctoproject.org/documentation

For more information about OpenEmbedded see their website:
http://www.openembedded.org/

You can now run 'bitbake <target>'

Common targets are:
core-image-minimal
meta-toolchain
meta-toolchain-sdk
adt-installer
meta-ide-support

Your configuration files at bld-fb/ have not been touched.

/////////////////////////////////////////////////////////////////////////////////

Your configuration files at bld-fb/ have not been touched.
imx6@ubuntu:bld-fb$ hob
No command 'hob' found, did you mean:
Command 'bob' from package 'python-sponge' (universe)
Command 'hnb' from package 'hnb' (universe)
Command 'hot' from package 'hopenpgp-tools' (universe)
Command 'hoz' from package 'hoz' (universe)
hob: command not found

Labels (2)
Tags (2)
0 Kudos
1 Reply

1,256 Views
joanxie
NXP TechSupport
NXP TechSupport

refer to the log file "Your configuration files at bld-fb/ have not been touched.", try to change to another to build, or just use the command " source ./setup-environment build"

0 Kudos