DDR Stress Test v2.70 issues

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DDR Stress Test v2.70 issues

615 Views
srikanthmediset
Contributor I

Hai,

  We are using iMX6sl EVK board and we are not able to boot the board with android 4.43 source.So we tried to do DDR stress test with v2.70 and v.1.0.3 versions but both of them are failing at calibration level.We are trying to do for DDR3 with 512 ram. So anyone can help me in this to resolve this issue or can any one provide i.Mx6SL DDR3 script file.

Regards,

srikanth.

Labels (2)
0 Kudos
2 Replies

439 Views
srikanthmediset
Contributor I

Hi,

  I tried with LPDDR2 script file then DDR stress test is running successfully upto calibration test.But when I am running stress test it is failing.I think previously I am running wrong script on my board.Now if I am going in correct way means how to overcome this error.Please give some suggestions.

Regards,

srikanth.

0 Kudos

439 Views
igorpadykov
NXP Employee
NXP Employee

Hi srikanth

ddr3 script for i.MX6SL EVK can be found in stress test v2.70

folder /script/mx6sl, also please look at FAQ section on

i.MX6/7 DDR Stress Test Tool V2.70 

and Freescale i.MX6 DRAM Port Application Guide-DDR3

Freescale i.MX6 DRAM Port Application Guide-DDR3 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos