I'm running Windows 10 in VirtualBox on Mac OSX.
With LPC Xpresso cannot connect to LPC link 2.
Looking in the Windows 10 "Devices and Printers" control panel there is a warning sign on the LPC Link 2 icon which leads to information as below.
All the drivers and sofware versions are the latest and have restarted.
Any suggestions please?
Device USB\VID_1FC9&PID_0090\JQD4FXOT had a problem starting.
Driver Name: usb.inf
Class Guid: {36fc9e60-c465-11cf-8056-444553540000}
Service: usbccgp
Lower Filters:
Upper Filters:
Problem: 0xA
Problem Status: 0xC000000D
(Windows 10 Screenshot attached too.)
First of all, I assume that you know that LPCXpresso IDE with LPC-Link2 will work natively on Mac OS X ?
Its also worth saying that our own experience of VirtualBox on Mac OS X was not very positive, from the USB support side of things (though that was a while ago). Our Mac OSX users now generally use VMWare, and increasingly Parallels to run Windows on Macs.
But that aside, try going through : LPC-Link2 fails to enumerate with CMSIS-DAP firmware
Its also possible that pre-programming the Link2 probe firmware rather than letting the IDE softload it might help : LPC-Link2 Debug Probe firmware programming
Regards,
LPCXpresso Support