Hello, now we have a project that needs your P1010 processor. Can you connect the Optical module directly to this processor? If so, which interface should I connect to?.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Hello, now we have a project that needs your P1010 processor. Can you connect the Optical module directly to this processor? If so, which interface should I connect to?.

486 Views
whao1005
Contributor I

  Hello, now we have a project that needs your P1010 processor. Can you connect the   Optical module directly to this processor? If so, which interface should I connect to?

Labels (1)
Tags (1)
0 Kudos
1 Reply

330 Views
r8070z
NXP Employee
NXP Employee


Have a great day,

I guess you mean a SFP module. Some SFP modules can be connected directly to the P1010 SGMII interface. The P1010 eTSEC SGMII interface was designed to connect the on-chip MAC to an SGMII compatible PHY. Therefore, NXP does not have specific recommendations for interfacing directly to an SFP optical transceivers readily available. There can be some problem with the direct connection - please see

https://community.nxp.com/thread/308353

https://community.nxp.com/thread/353124

Both discussions are valid for the P1010 SGMII. However there are also SGMII SFP optical transceiver which has built-in PHY supporting SGMII Interface, see for example
SGMII SFP Optical Transceivers(100BASE-FX/LX) - Xmultiple 

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos