i.MX6ULL read and write fusemap

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

i.MX6ULL read and write fusemap

3,144 Views
mannsikchung
Contributor III

Dear All.

The addresses of fusemap are 0x400, ...., 0x450, 0x460, 0x470, 0x6D0, etc.

And, only part of 0x450 is accessable by H/W BOOT_CFG pins.

How to access 0x430[21:20] from software or bootloader?

"md" command of u-boot is usable?

I want to read current setting of 0x430[21:20], TAMPER_PIN_DISABLE.

And, I want to change 0x430[21:20]. How can I change it?

BR.

Mannsik

Labels (3)
0 Kudos
4 Replies

384 Views
keyur-mpc
Contributor I

Have you found the solution?

0 Kudos

1,967 Views
brenolima
NXP Employee
NXP Employee

Hi mannsikchung‌,

You can use the fuse API in u-boot for reading and writing:

=> fuse read <bank> <word> [<cnt>]
=> fuse prog [-y] <bank> <word> <hexval>

You can find more details about it and a example in the following link: Burning eFuses on i.MX6 and i.MX7 - i.MXDev Blog 

Thanks,

Breno Lima

0 Kudos

1,967 Views
art
NXP Employee
NXP Employee

What exactly i.MX series processor do you mean? Please specify it first.

Best Regards,

Artur

0 Kudos

1,967 Views
mannsikchung
Contributor III

As the title says, I'm using i.MX6ULL.

0 Kudos