Does CS0 of i.MX6D support 4GB DDR3?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does CS0 of i.MX6D support 4GB DDR3?

Jump to solution
516 Views
hi_shawn
Contributor II

Hi guys,

One of my customer wants to use 4 GB DDR3 for new project. According the i.MX6Q SABRE-SDB EK schematic, can i replace the 2G_DDR3_SDRAM_128MX16 with 8G_DDR3_SDRAM_512MX16 to meet customer's requirement? For example, 4 * MT41K512M16HA-125.

Labels (1)
0 Kudos
1 Solution
380 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shawn

yes it is supported. Also one can look at

4GB DDR3 Support https://community.nxp.com/thread/384856 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

View solution in original post

1 Reply
381 Views
igorpadykov
NXP Employee
NXP Employee

Hi Shawn

yes it is supported. Also one can look at

4GB DDR3 Support https://community.nxp.com/thread/384856 

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------