mkm33z128aclh5

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

mkm33z128aclh5

1,391 Views
dporada
Contributor III
I'm planning on using a mkm33z128aclh5 in a new product and I'm not sure which IDE to use. The produce page suggests MCUXpresso, but when I try to use the pin tools, it only has one device of the family listed.
0 Kudos
3 Replies

1,249 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Don,

You can use KDSv3.2, CWv10.7 or IAR. KDS is free.

And then  download the kinetis M bare-metal drivers to development your project.

ARM Cortex-M0+|Kinetis KM3x 50-75 MHz 32-bit MCUs|NXP 

pastedImage_1.png

Hope it helps


Have a great day,
TIC

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,249 Views
dporada
Contributor III

Is there any way to make a processor expert project?

Thank you,

Don Porada

0 Kudos

1,248 Views
Alice_Yang
NXP TechSupport
NXP TechSupport

Hello Don,

Sorry the Processor Expert doesn't support KM series product.

BR

Alice

0 Kudos