Expresso BLDC motor controller with LPC40xx processor

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Expresso BLDC motor controller with LPC40xx processor

1,044 Views
billbrown
Contributor I

an I marry a OM13068: LPC1549 LPCXpresso Motor Control Kit (BLDC) board to something other than a LPC Expresso LPC15xx processor board? Specifically I would like to use an LPC40xx Processor. Is there an LPC40xx Expresso board that will attach to the BLDC motor controller board?

Tags (1)
0 Kudos
1 Reply

852 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hello Bill Brown,

   About the BLDC for LPC chip.

  I just find the LPC1549 and LPC1700.

 LPC1549 LPCXpresso Motor Control Kit (BLDC)|NXP 

http://cache.nxp.com/docs/en/application-note/AN10898.zip?fsrch=1&sr=1&pageNum=1 

So, if you want to use LPC40xx, maybe you need to refer to the LPC1549 board and design it by yourself.

Wish it  helps you!


Have a great day,
Kerry

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos