MCUXpresso IDE and Kinetis devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MCUXpresso IDE and Kinetis devices

1,555 Views
rodrigocavalcan
Contributor I

Hi,

   I'm starting the work with MKM34z and I'm switching to use the MCUXpresso for it. I already use the MCUXpresso for LPC devices. I cannot find any Kinetis family device on the list when I try to create the project. I already re-installed the IDE and switched to a new workspace. When I try to use the MCUXpresso Config Tools, I can see only a subset of Kinetis devices. On this list I can see the MKM34256xxx7, but not other variant with the 100 pins.

   Now I don't know if I'm supposed to use the new MCUXpresso, if it have support for these parts, or if I have to continue using the KDS IDE.

   Please enlighten me,

   Thanks,

   - Rodrigo

Labels (1)
Tags (1)
0 Kudos
1 Reply

890 Views
ZhangJennie
NXP TechSupport
NXP TechSupport

Hi Rodrigo.

So far, MCUXpresso only supports parts of kinetis project.

here is MCUXpresso Supported Devices Table for reference

MCUXpresso Supported Devices Table 


Have a great day,
Jennie Zhang

-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos