I am currently learning how to use the MCB4300 Evalution board with the LPC4357 microcontroller.
I have got Keil uvision working, and the blinky example loaded onto the board.
I have been studying the example and using the user manual to try and understand how to program the microcontroller. I know understand things such as setting the clock for a GPIO port, setting the function of a pin and setting its direction.
I am now unsure how I would read a digital input, the user manual lists some options, however from reading the data sheet I am unsure how to implement this.
Is there any code examples other than blinky, which I can learn from while also referring back the the user manual or any other ways of learning how to program the LPC4357?
Thanks
Hi,
Please check the below, in this doc a LPC11u24 is used, however the process is the same for other LPC's.
I hope this helps.
https://community.nxp.com/docs/DOC-333169
Have a great day,
Sol
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------