XIP perfomrance versus internal FLASH in LPC546xx

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

XIP perfomrance versus internal FLASH in LPC546xx

694 Views
Jetcitycowboy
NXP Employee
NXP Employee

Do you know how the execution time of the XIP (execute in place) feature of SPIFI on the LPC546xx parts would compare to  internal flash and also to the MK22FN512 executing code from internal flash?

Labels (1)
0 Kudos
1 Reply

391 Views
Carlos_Mendoza
NXP Employee
NXP Employee

Hi Kenneth,

You can refer to the "SPIFI Performance" section in the following presentation for more information. It compares the effective throughput for different flash types and there is a table showing the coremark performance results for the different memory locations:

https://community.nxp.com/docs/DOC-333596 


Hope it helps!

Best Regards,
Carlos Mendoza
Technical Support Engineer

0 Kudos