Hello to those concerned,
I'm trying to build MQX4.2 with GT202 Atheros support. I've installed MQX4.2. I've applied the 4.2.0.2 patch. I've turned on the BSPCFG_ENABLE_ATHEROS_WIFI as well as BSP_ENET_WIFI_ENABLED. I've copied the Atheros drivers into the MQX distribution.
When I build, I am getting these errors:
C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c: In function 'fill_scan_info':
C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c:59:16: error: 'ENET_SCAN_INFO' has no member named 'rsn_cipher'
C:/Freescale/Freescale_MQX_4_2/mqx/source/io/enet/atheros_wifi/custom_src/api_interface/cust_api_wmi_rx.c:63:16: error: 'ENET_SCAN_INFO' has no member named 'rsn_cipher'
Am I missing a support patch for MQX4.2 which is required for the GT202 driver?
Hi Eric:
Unfortunately GT202 is developed by our partner Qaulcomm-Atheros, I would suggest you contact with Qualcomm directly.
However, please check the below thread, in this thread you will find an example of porting the web_hvac demo app to use GT202
https://community.nxp.com/docs/DOC-102702
I hope it helps
Have a nice day!
Regards
Daniel