Unable to connect to the core on LPC1549

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Unable to connect to the core on LPC1549

1,106 Views
gergosnoo
Contributor II

I am using LPC1549 and as a beginner, I tried to run one of the given example projects after I imported them.

I got the following error : Failed on connect: Ee(36). Could not connect to core.

Since I installed lpcxpresso, I did not modify anything in the user environment. I only plugged my lpc1549 on USB and tried to run blinky and then other projects, but I got the same error every time.

The attached picture shows the error.

Please let me know how can I connect to my core properly!

Best Regards, 

Gergo

Labels (1)
0 Kudos
3 Replies

793 Views
gergosnoo
Contributor II

I had to change the Jumper position on the board and then the connection to core problem is solved.

Thanks for help.

0 Kudos

793 Views
lpcxpresso_supp
NXP Employee
NXP Employee

In the first place, please check your debug/reset circuitry against : Design Considerations for Debug 

If you are still having problems, then please provide some more details about your board, IDE version, debug probe and host operating system.

It would also be helpful if you could post the actual text from the IDE's debug console when your debug session fails:  The Debug Log 

Regards,

LPCXpresso Support

0 Kudos

793 Views
converse
Senior Contributor V

Have you connected the SWD cable the correct way around? Have you powered the board correctly? Either of these can cause your problem.

0 Kudos