Availability of Unused Camera Parallel interface lines as GPIO's

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Availability of Unused Camera Parallel interface lines as GPIO's

Jump to solution
447 Views
harishs
Contributor I

Hi,

I would like to know whether the unused lines in 20 bit camera parallel interface of IMX6 Quad core processor can be used as normal GPIO lines. In my case i am interfacing a 10 bit monochrome image sensor to D19 to D10 lines of CPI interface.The data will be captured in 16 bit generic mode,my query is whether the unconnected 6 LSB bits when data is acquired in 16 bit generic mode can be used as normal GPIO lines. 

Regards,

Harish.S

Labels (1)
0 Kudos
1 Solution
372 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, it is possible to configure the unused Camera interface pins for GPIO.

When configuring GPIO, Pin tools  may be useful.

Pins Tool for i.MX Application Processors|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

View solution in original post

0 Kudos
1 Reply
373 Views
Yuri
NXP Employee
NXP Employee

Hello,

  yes, it is possible to configure the unused Camera interface pins for GPIO.

When configuring GPIO, Pin tools  may be useful.

Pins Tool for i.MX Application Processors|NXP 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct Answer

button. Thank you!

0 Kudos