Can i use 1xCSI and 3xMIPI to support 1x720P and 3xD1 video sulotion in IMX6Q

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Can i use 1xCSI and 3xMIPI to support 1x720P and 3xD1 video sulotion in IMX6Q

746 Views
lijie2045
Contributor II

Hi all,

I saw below message below at  iMX6DQ ISL79985/79987 MIPI CSI2 CVBS camera surround view solution for Linux BSP :

The attached patch can make the BSP support up to 4 cameras based on 3.10.53 GA 1.1.0 BSP.

 The 4 cameras can be:

- 1xCSI, 3xMIPI

- 2xCSI, 2xMIPI

- 4xMIPI

it  supports  4XD1 video

But in my case ,i need it supports  3XD1 and 1X720P cameras input at the same time.

then ,Can i use  1xCSI, 3xMIPI ?1 csi for 720p and 3XMIPI for D1?

can it  work at the same time?

TKS

0 Kudos
2 Replies

541 Views
igorpadykov
NXP Employee
NXP Employee

Hi

in general yes, it is possible to use use  1xCSI, 3xMIPI ?1 csi for

720p and 3XMIPI for D1 at the same time.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

541 Views
lijie2045
Contributor II

TKS.

can an parallel CSI be multiplexed?

0 Kudos