Hi,
In Imx6ull processor has internal 4/5 wire Resistive Touchscreen Controller so we don't require to use External TSC part through I2C/SPI communication as per my understanding.
Following are the signals used for TSC of LCD module. could you please provide the expansion of ynlr,ypll,xnur, xpul pin names.
I check with the reference design NXP EVK, I have doubt on the xnur, xpul signal connection. Please clarify us
As per my understanding :
xnur - X negative upper right side
xpul - X positive upper left side
ynlr - Y negative lower right side
ypll - Y positive lower left side
Is it correct?
Thanks Igor
Hi ramesh
I think it is correct, unfortunately I am not aware of additional TSC documentation.
May be useful to check lcd datasheet which is used with i.MX6UL EVK board
Detail datasheet of LCD8000-43T
Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
So I hope it will work directly to LCD which has those 4 signals. Am i right?
Or shall we need to add any buffer circuit inbetwenn SOC and LCD for touch screen signals?
>it will work directly to LCD which has those 4 signals. Am i right?
right
Best regards
igor