IMX6UL wm8960 used SAI1 failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

IMX6UL wm8960 used SAI1 failed

3,094 Views
jiangzhifei
Contributor I

#Hello,

 

I encounter an audio problem on our IMX6UL board.

But the board uses SAI1,  it's different from IMX6ULEVK which uses SAI2.

I  use ALSA "aplay" utility  to test.

But can't play successfully.

error message:

aplay -D "plug:SLAVE='hw:0,0'" /test/test.wav
Playing WAVE '/test/test.wav' : Signed 16 bit Little Endian, Rate 22050 Hz, Stereo
aplay: pcm_write:1682: write error: Input/output error

 

I will be appreciated if someone can help to fix the issue.

Thanks.

kernel start message:

...

[ 5.359750] imx-wm89601 sound1.14: wm8960-hifi <-> 2028000.sai mapping ok
[ 5.368187] imx-wm89601 sound1.14: snd-soc-dummy-dai <-> 2034000.asrc mapping ok
[ 5.375877] imx-wm89601 sound1.14: wm8960-hifi <-> 2028000.sai mapping ok
...
[ 5.575216] ALSA device list:
[ 5.578342] #0: wm8960-audio

Our DTS configuration is modified as below.

IMX6UL.dtsi:

sai1: sai@02028000 {
   compatible = "fsl,imx6ul-sai";
   reg = <0x02028000 0x4000>;
   interrupts = <GIC_SPI 97 IRQ_TYPE_LEVEL_HIGH>;
   clocks = <&clks IMX6UL_CLK_SAI1_IPG>,
   <&clks IMX6UL_CLK_SAI1>,
   <&clks 0>, <&clks 0>;
   clock-names = "bus", "mclk1", "mclk2", "mclk3";
   dma-names = "rx", "tx";
   dmas = <&sdma 35 25 0>, <&sdma 36 25 0>;
   status = "disabled";
};

imx6ul-14x14-evk-7.dts:

sound {
   compatible = "fsl,imx6ul-evk-wm8960",
   "fsl,imx-audio-wm8960";
   model = "wm8960-audio";
   cpu-dai = <&sai1>;
   audio-codec = <&codec1>;
   asrc-controller = <&asrc>;
   codec-master;
   gpr = <&gpr>;
   audio-routing =
   "Headset Jack", "HP_L",
   "Headset Jack", "HP_R",
   "Ext Spk", "SPK_LP",
   "Ext Spk", "SPK_LN",
   "Ext Spk", "SPK_RP",
   "Ext Spk", "SPK_RN",
   "LINPUT2", "Hp MIC",
   "LINPUT3", "Hp MIC",
   "RINPUT1", "Main MIC",
   "RINPUT2", "Main MIC",
   "Hp MIC", "MICB",
   "Main MIC", "MICB",
   "CPU-Playback", "ASRC-Playback",
   "Playback", "CPU-Playback",
   "ASRC-Capture", "CPU-Capture",
   "CPU-Capture", "Capture";
};

&sai1 {
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_sai1>;

   assigned-clocks = <&clks IMX6UL_CLK_SAI1_SEL>,
   <&clks IMX6UL_CLK_SAI1>;
   assigned-clock-parents = <&clks IMX6UL_CLK_PLL4_AUDIO_DIV>;
   assigned-clock-rates = <0>, <11289600>;

   status = "okay";
};

pinctrl_sai1: sai1grp {
   fsl,pins = <
      MX6UL_PAD_CSI_DATA01__SAI1_MCLK 0x17088
      MX6UL_PAD_CSI_DATA05__SAI1_TX_BCLK 0x17088
      MX6UL_PAD_CSI_DATA07__SAI1_TX_DATA 0x11088
      MX6UL_PAD_CSI_DATA04__SAI1_TX_SYNC 0x17088
      MX6UL_PAD_CSI_DATA06__SAI1_RX_DATA 0x11088
   >;
};

Labels (1)
0 Kudos
9 Replies

1,356 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiang

please also check i2c entry and change clock appropriately:

&i2c2 {   ..

    codec: wm8960@1a {
        compatible = "wlf,wm8960";
        reg = <0x1a>;
        clocks = <&clks IMX6UL_CLK_SAI2>;
        clock-names = "mclk";
        wlf,shared-lrclk;
    };

may be recommended to check sai clocks with oscilloscope

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 Kudos

1,356 Views
jiangzhifei
Contributor I

Hi igorpadykov

Thank you for your reply!

 

my i2c set:

&i2c2 {
   clock_frequency = <100000>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_i2c2>;
   status = "okay";

   codec1: wm8960@1a {
      compatible = "wlf,wm8960";
      reg = <0x1a>;
      clocks = <&clks IMX6UL_CLK_SAI1>;
      clock-names = "mclk";
      wlf,shared-lrclk;
   };

};

pinctrl_i2c2: i2c2grp {
   fsl,pins = <

      MX6UL_PAD_UART5_TX_DATA__I2C2_SCL 0x4001f8a8
      MX6UL_PAD_UART5_RX_DATA__I2C2_SDA 0x4001f8a8
   >;
};

Is there something wrong?

I'll check all the signals with an oscilloscope if my set is all correct...

0 Kudos

1,356 Views
igorpadykov
NXP Employee
NXP Employee

could you confirm that mclk is present on codec.

Best regards
igor

0 Kudos

1,356 Views
jiangzhifei
Contributor I

Hi igorpadykov

my sai1 mclk pin is CSI_DATA01,but I couldn't detect the signal when I started playing!

Is there any error in the following settings?

&i2c2 {
   clock_frequency = <100000>;
   pinctrl-names = "default";
   pinctrl-0 = <&pinctrl_i2c2>;
   status = "okay";

   codec1: wm8960@1a {
      compatible = "wlf,wm8960";
      reg = <0x1a>;
      clocks = <&clks IMX6UL_CLK_SAI1>;
      clock-names = "mclk";
      wlf,shared-lrclk;
   };

};

 

0 Kudos

1,356 Views
igorpadykov
NXP Employee
NXP Employee

Hi jiang

one can try to find reason for absence mclk, please attach jtag

(or add debug printfs) and check sai1 gate bits in CCM_CCGR5,

bit MSEL in I2Sx_TCR2, I2Sx_RCR2 and iomux settings for CSI_DATA01

also try

MX6UL_PAD_CSI_DATA01__SAI1_MCLK 0x1b088

Best regards
igor

0 Kudos

1,356 Views
jiangzhifei
Contributor I

Hi igorpadykov

I read CCM_CCGR5, value is 0xc3ffc3ff,

29–28 bit is 00
CG14 sai1 clock (sai1_clk_enable) is 00 

00 Clock is off during all modes. Stop enter hardware handshake is disabled.

So i write 0xff3ffc3ff to CCM_CCGR5,but mclk on sai1 ( CSI_DATA01 pin ) is still no signal.

how to make a correct set?  thanks a lot !

ps:

I try to read I2Sx_TCR2, I2Sx_RCR2 too , but read failed,so I can not check them:

test code:

#define SAI_START 0x2028000
#define CCM_CCGR5 0x20C407C

void test_sai_1(void){
   void __iomem *jzf_io;
   int count = 36;
   u32 cfg;
   int i;

   jzf_io = ioremap(CCM_CCGR5,sizeof(u32));
   cfg = readl(jzf_io);
   printk(KERN_ALERT"get CCM_CCGR5 value = 0x%x\n",cfg);
   cfg = 0xf3ffc3ff;
   writel(cfg,jzf_io);
   cfg = readl(jzf_io);
   printk(KERN_ALERT"get CCM_CCGR5 value = 0x%x\n",cfg);
   iounmap(jzf_io);


   jzf_io = ioremap(SAI_START,sizeof(u32)*count);
   for(i = 0; i < count; i++){
      cfg = readl(jzf_io+i*sizeof(u32));
      printk(KERN_ALERT"get value = 0x%x\n",cfg);
   }
   iounmap(jzf_io);

}

test print:

[ 356.512952] get CCM_CCGR5 value = 0xc3ffc3ff
[ 356.518408] get CCM_CCGR5 value = 0xf3ffc3ff
[ 356.523665] get value = 0x0
[ 356.528536] get value = 0x0
[ 356.531363] get value = 0x0
[ 356.534170] get value = 0x0
[ 356.537810] get value = 0x0
[ 356.540634] get value = 0x0
[ 356.543442] get value = 0x0
[ 356.547347] get value = 0x0
[ 356.550165] get value = 0x0
[ 356.552969] get value = 0x0
[ 356.556419] get value = 0x0
[ 356.559233] get value = 0x0
[ 356.562036] get value = 0x0
[ 356.564838] get value = 0x0
[ 356.568223] get value = 0x0
[ 356.571039] get value = 0x0
[ 356.573844] get value = 0x0
[ 356.577189] get value = 0x0
[ 356.580002] get value = 0x0
[ 356.582804] get value = 0x0
[ 356.586078] get value = 0x0
[ 356.588891] get value = 0x0
[ 356.591696] get value = 0x0
[ 356.594497] get value = 0x0
[ 356.597847] get value = 0x0
[ 356.600661] get value = 0x0
[ 356.603463] get value = 0x0
[ 356.606733] get value = 0x0
[ 356.609548] get value = 0x0
[ 356.612350] get value = 0x0
[ 356.615153] get value = 0x0
[ 356.618488] get value = 0x0
[ 356.621299] get value = 0x0
[ 356.624101] get value = 0x0
[ 356.627352] get value = 0x0
[ 356.630164] get value = 0x0

0 Kudos

1,356 Views
igorpadykov
NXP Employee
NXP Employee

please debug sai driver, additional info can be found in Linux Manual

included in Doc package

http://www.nxp.com/webapp/Download?colCode=L4.1.15_2.0.0-LINUX-DOCS&Parent_nodeId=133769948107170617... 

Best regards
igor

0 Kudos

1,356 Views
jiangzhifei
Contributor I

Hi igorpadykov

I add some debug print in fsl_sai.c,when i use aplay to play music, i can read I2S1_RCR2 and CCM_CCGR5 value:

root@freescale ~$ aplay -D "plug:SLAVE='hw:0,0'" /test/test.wav

......

[ 293.554447] get CCM_CCGR5 value = 0x33ffc3ff
[ 293.558775] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCSR = 90000000
[ 293.564564] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCR1 = 0
[ 293.569743] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCR2 = 42000000
[ 293.575528] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCR3 = 0
[ 293.580709] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCR4 = 1a
[ 293.585974] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RCR5 = 0
[ 293.591155] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RDR = 0
[ 293.596250] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RFR = 0
[ 293.601340] !!!!!!!!!!!!!!!!!! 4 get FSL_SAI_RMR = 0

......

CCM_CCGR5  29–28 bit is 11 seems right.

bit MSEL in I2S1_RCR2 is 00

00 Bus Clock selected.
01 Master Clock (MCLK) 1 option selected.
10 Master Clock (MCLK) 2 option selected.
11 Master Clock (MCLK) 3 option selected.

iomux settings for CSI_DATA01

is

MX6UL_PAD_CSI_DATA01__SAI1_MCLK 0x1b088

my sai1 mclk pin is CSI_DATA01,but I couldn't detect the signal when I started playing too!

Do I need to change bit MSEL in I2S1_RCR2 value to try? 

0 Kudos

1,356 Views
igorpadykov
NXP Employee
NXP Employee

for MSEL please check
https://community.nxp.com/thread/448461

Best regards
igor

0 Kudos