Hi,
when I try to suspend attached debug session, I get a popup with message "Target request failed: HC/RS/S12Z GDI Protocol Adapter: Stop failed. Non Fatal Error." (screenshot attached). When I download and then suspend the application everything works fine (I can step through the application ...).
- CodeWarrior 10.7 (Eclipse)
- PEmicro Universal Multilink Rev B (green).
- S12Z 64k
What is the reason for that error popup and how to suspend attached debug session correctly?
Additional information: The application reset vector is not VECTOR 0. Does it have something to do with that?
Thank you very much!
Solved! Go to Solution.
Hi!
I found the problem! The VECTOR address has to be "four bytes aligned".
works: VECTOR ADDRESS 0xFFFFFD _Startup
does not work: VECTOR ADDRESS 0xFFFFFC _Startup
Hope it helps someone!
Hi!
I found the problem! The VECTOR address has to be "four bytes aligned".
works: VECTOR ADDRESS 0xFFFFFD _Startup
does not work: VECTOR ADDRESS 0xFFFFFC _Startup
Hope it helps someone!
Hi Nikolai,
Thank you for this question and also answer.
Yes, the S12Z vectors have 4 bytes while the addresses are just 3 bytes (24bit address space). So, the lowest byte from a vector is unused.
I use PE code for generating user vector table:
/* ISR prototype */
typedef void (* tIsrFunc)(void);
/* Pack 3 byte pointers as 4 byte Interrupt Vector Table entries */
typedef struct
{
byte padding;
tIsrFunc address;
} InterruptTableEntry;
#define _VECTOR(v) {0xFFU, &v}
//Please replace aprropriate Unimplemented_ISR by implemented interrupt routine
//see Table 1-13. Interrupt Vector Locations in RM for more details
InterruptTableEntry _InterruptVectorTable[INT_VECTOR_TABLE_SIZE] @INT_VECTOR_TABLE_ADDR = { /* Interrupt vector table */
_VECTOR(Unimplemented_ISR),//0x10
_VECTOR(Unimplemented_ISR),//0x14
_VECTOR(Unimplemented_ISR),//0x18
//…
I hope it helps you.
Have a great day,
Radek
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------