Does the Full Featured i.MX 6ULL also feature EPDC?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the Full Featured i.MX 6ULL also feature EPDC?

827 Views
peterlischer
Senior Contributor I

According to the part number nomenclature in section 1.1 of the datasheet, there are the following different parts available:

0: Baseline

1: General Purpose 1 (Reduced Feature)

2: General Purpose 2 (Full Feature)

7: With EPDC

Does "full featured" mean that really all features are included or is the EPDC interface excluded for these devices? In the ordering information table, for the full featured MCIMX6Y2DVM05AA the EPDC interface is not listed. 

Tags (2)
0 Kudos
1 Reply

599 Views
gusarambula
NXP TechSupport
NXP TechSupport

Hello Peter Lischer,

Full Featured means all features except for the EPDC, which is listed separately. Part numbers with EPDC are not “Full Featured” since they do not have all the modules of the “Full Featured” part numbers.

I understand the confusion since EPDC is handled separately and “Full Feature” leaves out the EPDC.

There are some examples on table 1 of the Datasheet that may help to illustrate this.

My apologies for the inconvenience! I hope this helps!

Regards,

0 Kudos