Hello,
I'm trying to validate a custom board with a T2080 device.
From codewarrior I can connect to the board and I can access all registers of T2080 processor (LAW, IFC, DDR, ...)
But when I start QCVS in order to use DDR validation toos I get a error "can't connect to server!"
And when I open Validation tab no Target connection is available
I've a valid license for this product.
The CCS server is working properly and detect CWTAP
Can tou help me?
thanks in advance.
Make sure you select Target access to localhost not remote. Also, try creating a new target connection.
Adrian
Hello,
When I select localhost, automatically changes to remote.
I can’t generate a new target connection, the button is disabled.
De: addiyi
Enviado el: miércoles, 10 de mayo de 2017 12:53
Para: Hernández Sánchez, Sergio
Asunto: Re: - Re: DDR validation tools can't connect to server
NXP Community <https://community.freescale.com/resources/statics/1000/35400-NXP-Community-Email-banner-600x75.jpg>
Re: DDR validation tools can't connect to server
reply from Adrian Stoica<https://community.nxp.com/people/addiyi?et=watches.email.thread> in CodeWarrior for QorIQ - View the full discussion<https://community.nxp.com/message/904078?commentID=904078&et=watches.email.thread#comment-904078>
Try to use a new workspace.
Adrian