AnsweredAssumed Answered

MPU FreeRTOS

Question asked by imanolallende on Apr 27, 2017
Latest reply on May 2, 2017 by imanolallende

I am using the i.MX 6SoloX board with a Linux image in the Cortex-A9 and FreeRTOS in Cortex-M4. I am trying to use the OCRAM as shared memory between both cores.

 

If we look to the memory maps tables, it can be seen that the A9 is  0x90000-0x91FFFF and M4 is  20900000-2091FFFF.

 

In Linux dtb I have set the following shared memory:

    fsl,shared-mem-addr = <0x91F000>;
    fsl,shared-mem-size = <0x1000>;

 

Therefore, in FreeRTOS I want to read the following memory range and I set the permission in the RDC. (hardware_init.c)

    uint32_t start, end;

    start = 0x20910000;
    end = 0x2091FFFF;

    RDC_SetMrAccess(RDC, rdcMrOcram, start, end, 0xFF, true, false);

 

If a I write something in the RAM memory, the only way I have get to read it through the Cortex-M4 is disabling the Cache memory in system_MCIMX6X_M4.c.

      LMEM_PSCCR = (LMEM_PSCCR_ENWRBUF_MASK /*| LMEM_PSCCR_ENCACHE_MASK*/);

 

However, I only want to disable it for the OCRAM, not for the whole system. I tried with the MPU but I do not get the desired result. I program it in region 1 with the following features (TEX 000 / C 1 / B 0 / S 1 / AP 011 / 64KB).

Why I do not get to read the data if I disable the cache for it? Do I disable it correctly?

 

    /* M4 core clock root configuration. */
    /* Initialize MPU */
    /* Make sure outstanding transfers are done. */
    __DMB();
    /* Disable the MPU. */
    MPU->CTRL = 0;

 

    /* Select Region 0 to configure DDR memory(1MB). */
    MPU->RNR  = 0;
    MPU->RBAR = 0x80000000;
    MPU->RASR = 0x030B0027;

 

    /* Select Region 1 to configure share memory with A9(1M). */
    MPU->RNR  = 1;
    MPU->RBAR = 0x20910000;
    MPU->RASR = 0x306001F;                                    


    /* Select Region 2 to configure ocram. */
    MPU->RNR  = 2;
    MPU->RBAR = 0;
    MPU->RASR = 0;


    /* Select Region 3 to configure QSPI memory. */
    MPU->RNR  = 3;
    MPU->RBAR = 0x60000000;
    MPU->RASR = 0x030B0029;

 

    /* Disable unused regions. */
    MPU->RNR  = 4;
    MPU->RBAR = 0;
    MPU->RASR = 0;
    MPU->RNR  = 5;
    MPU->RBAR = 0;
    MPU->RASR = 0;
    MPU->RNR  = 6;
    MPU->RBAR = 0;
    MPU->RASR = 0;
    MPU->RNR  = 7;
    MPU->RBAR = 0;
    MPU->RASR = 0;

 

    /* Enable Privileged default memory map and the MPU. */
    MPU->CTRL = MPU_CTRL_ENABLE_Msk |
             MPU_CTRL_PRIVDEFENA_Msk;
    /* Memory barriers to ensure subsequence data & instruction
    * transfers using updated MPU settings.
    */
    __DSB();
    __ISB()

Outcomes