Hello,
Is there any NXP product (active) with similar features to this?
I need work in 868Mhz ISM
I need Long Range and operation between 500mW-1W and 3~5V
For used with small antenna. Actually I used this antenna of 120mm.
Network topology: Point-to-Multipoint
SPI, I2C or UART interface for the mcu.
Multipoint (or endDevice) requeriments:
Power supply: 12V DC typical. I used dc/dc buck converter for 3V3 or 5V but I could use 12V if it gets more reach
Multiple 12V buses: 3A, 5A, 10A, 15A, 20A and 30A (protec with littlefuse mini fuse auto).
At least 1 GPIO if it's possible. Otherwise I have to use Kinetis mcu, L series for example.
Point (or coordinator) requeriments:
Power supply: 1.5V ~ 5V (AA batteries with dc/dc boost/buck converter with dedicated Low-noise LDO for the transmitter).
SPI, I2C or UART interface to K series MCU.
If you need more details, please let me know.
Sorry for my english.
Thanks and regards.
Solved! Go to Solution.
I found the OL2835. I think it can work to me.