Install McuExpress in Ubuntu 17

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Install McuExpress in Ubuntu 17

Jump to solution
1,110 Views
javierhernande1
Contributor IV

Hello,

I have installed KDS 3.0.2 but now I want to install mcuxpressoide-10.0.0_344.x86_64 but I have a conflict with KDS 3.0.2.

I have removed /lib/udev/rules.d/55-pemicro.rules but not works. Any idea how to fix it?

sudo ./mcuxpressoide-10.0.0_344.x86_64.deb.bin
Verifying archive integrity... All good.
Uncompressing mcuxpressoide installer 100%
Installing...
(Leyendo la base de datos ... 412401 ficheros o directorios instalados actualmente.)
Preparando para desempaquetar JLink_Linux_x86_64.deb ...
Removing /opt/SEGGER/JLink ...
/opt/SEGGER/JLink not found (OK)
Desempaquetando jlink (6.14) sobre (6.14) ...
Configurando jlink (6.14) ...
(Leyendo la base de datos ... 412401 ficheros o directorios instalados actualmente.)
Preparando para desempaquetar mcuxpressoide-10.0.0_344.x86_64.deb ...
Desempaquetando mcuxpressoide (10.0.0) ...
dpkg: error al procesar el archivo mcuxpressoide-10.0.0_344.x86_64.deb (--install):
intentando sobreescribir `/lib/udev/rules.d/55-pemicro.rules', que está también en el paquete kinetis-design-studio 3.2.0
Procesando disparadores para bamfdaemon (0.5.3+17.04.20170406-0ubuntu1) ...
Rebuilding /usr/share/applications/bamf-2.index...
Procesando disparadores para gnome-menus (3.13.3-6ubuntu5) ...
Procesando disparadores para desktop-file-utils (0.23-1ubuntu2) ...
Procesando disparadores para mime-support (3.60ubuntu1) ...
Se encontraron errores al procesar:
mcuxpressoide-10.0.0_344.x86_64.deb
Leyendo lista de paquetes... Hecho
Creando árbol de dependencias
Leyendo la información de estado... Hecho
E: El paquete kinetis-design-studio necesita ser reinstalado, pero no se encuentra el archivo para ello.

Labels (1)
0 Kudos
1 Solution
599 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Javier,

if you still need to run both KDS and MCUXpresso on the same machine please look for this thread:

https://community.nxp.com/thread/447699 

MCUXpresso support

View solution in original post

3 Replies
600 Views
lpcxpresso_supp
NXP Employee
NXP Employee

Hi Javier,

if you still need to run both KDS and MCUXpresso on the same machine please look for this thread:

https://community.nxp.com/thread/447699 

MCUXpresso support

599 Views
javierhernande1
Contributor IV

Thank u!

0 Kudos
599 Views
javierhernande1
Contributor IV

I solved it by uninstalling KDS

sudo dpkg -r kinetis-design-studio

and now works, but is there any way to have both installs on Ubuntu? (KDS and McuExpesso) (As I have in Windows 8.1)

Regards

0 Kudos