While connecting the board with codewarrior, as I run the cwflash.py script inside the gdb I'm getting the following error, "CCS: cc config string invalid and GTA: target connection error". What is the cause for the above error?
Hello emacs bala,
Probably you didn't specify the correct Connection probe parameter, please refer to comments in this script to assign a valid probe type.
# Connection probe. Possible values:
# PROBE_CONNECTION = "" - use local CWTAP through USB.
# PROBE_CONNECTION = "<serial_number>" - use local CWTAP USB with specified serial number. Ex: "12:34:56:78:9a:bc"
# PROBE_CONNECTION = "<IP>|<host_name>" - use remote CWTAP
# PROBE_CONNECTION = "cmsisdap[:<serial_number>]" - use CMSIS-DAP with or without serial number
PROBE_CONNECTION = ""
In addition, please update to the latest CodeWarrior version, you could use IDE to do flash programming.
Please refer to Use CodeWarrior for ARMv8 to Debug U-boot and Linux Kernel and Bring up Bare Boards.
Have a great day,
Yiping
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
I did it through USB, so didn't give any value to that variables
Please update to the latest CW4NET2017.03. You can find the installation package on nxp.com.
Adrian
Please provide the CW version (go to Help > About CodeWarrior...).
Adrian
I'm using this on Linux os.
CW4NET_V2016.01 is the dir name.