OV7740 camera porting on IMX6ULEVK

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

OV7740 camera porting on IMX6ULEVK

903 Views
raghavendrabork
Contributor II

Hi, 

So far we could find some references with OV7740 Solo/DL. We are porting OV7740 on #imx6ulevk and looking for references with Yocto build.

We understand that, UL does not uses IPU and instead PXP is used for image processing processing. (Ref: how to rorate lcd screen 90 degree for IMX6UL in linux kernel or linux driver? ) and imx6ul reference manual.

Some more discussions we have checked:

ov7740 camera with custom i.MX6DL board using CSI0 in HREF (gated clock) mode 

OV7740 camera on I.MX6 using CSI0 in BT.656 mode 

But could not able to get exact code reference. We want to have some source code reference or patch for UL EVK.

Please let us know if anything similar can be used for integration. 

Regards,

-Raghu

Labels (3)
1 Reply

537 Views
igorpadykov
NXP Employee
NXP Employee

Hi Raghavendra

one can check drivers in ..drivers/media/platform/mxc/subdev

linux-imx.git - i.MX Linux Kernel 

About preview function in i.MX6SL. 

and create service request for obtaining additional info.

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------