I am trying to enable OpenCL support both in the target image as well as the SDK built using populate_sdk. I am currently using the imx-3.14.28-1.0.0_ga BSP. I have a "minimal" build working without OpenCL. I don't have any gui elements included. I would like to know what I might need to add in the way of layers and/or conf instructions to get OpenCL support using the vivante GPU enabled. I really don't need wayland, x11, directfb etc.... Just GPU + OpenCL support. I hope some expert with yocto+imx might have some clues for me....Thanks.
Solved! Go to Solution.
I figured out some basics that have helped, but I still had to include directfb in my image.
Changed my conf to have:
DISTRO_FEATURES_remove = "x11 wayland"
DISTRO_FEATURES_append = " directfb"
Added this to my IMAGE_INSTALL:
packagegroup-core-directfb
fsl-gpu-sdk
I figured out some basics that have helped, but I still had to include directfb in my image.
Changed my conf to have:
DISTRO_FEATURES_remove = "x11 wayland"
DISTRO_FEATURES_append = " directfb"
Added this to my IMAGE_INSTALL:
packagegroup-core-directfb
fsl-gpu-sdk
Hi Terry
Also make sure that you have the graphics recipe and you are able to run those graphics unit test and fsl-gpu-sdk demos.
Also something to take in mind https://community.nxp.com/thread/428397
regards