Hello,
I'm trying to program a MCS568355 with the codewarrior usb tap in windows 8. The usb tap seems to work properly but I get an error message when trying to program the board with 56800E Flash programmer. The message is:
CCCSClient::ResetToDebug: Debug Mode
I really need to fix that, thanks.
Original Attachment has been moved to: Log.log.zip
Hi Sergio.
56800E Flash programmer v1.2 doesn't support win8 system. did you test it with a 32bit windows xp platform?
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------
Hello,
I have updated the flash programmer with the patch and upgraded my drivers but I suppose that it doesn't work anyway. The most annoying thing is that i have programmed my board 2/3 times succesfully trying about 50 times.
Now, I have to ask, ¿Is there any method to program my device under the modern versions of windows? ¿Can I program my device with another version of flash programmer or something like that under win8 using codewarrior usb tap?
Thanks for your help.
Hi Sergio,
CW10.7 includes simple flash that can work on win8.
here is CW10.7
CodeWarrior for Microcontrollers-Eclipse IDE|NXP
Here is how to use simple flash.
Standalone Flash Programmer | MCU on Eclipse
Have a great day,
Jennie Zhang
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------